PKR39809-02

Appendix E ­ IEEE Inverse Time Protection Tables

The times shown for the inverse time curves in this appendix are calculated according to the formulas defined in the IEEE Standard.

  • Standard Moderately Inverse = (0.0515 / (I^0.02 - 1)) + 0.114

  • Standard Very Inverse = (19.61 / (I^2-1)) + 0.491

  • Standard Extremely Inverse = (28.2 / (I^2-1)) + 0.1217

Where I is the fault current expressed as a multiple of the setting current.

Each curve is defined in terms of a formula such as:

Time = T / (IN – Q) + B

Where:

T = time parameter specific to characteristic

I = ratio of fault current to setting current

N = parameter specific to characteristic

Q = parameter specific to characteristic

B = parameter specific to characteristic

Tables for the times to trip for each of these curves are shown in the table below.

Table 105 IEEE Inverse Curves Timing Table

Setting Current Multiple

Standard Moderately Inverse Time (s)

Standard Very Inverse Time (s)

Standard Extremely Inverse Time (s)

1.10

27.11

93.87

134.41

1.50

6.44

16.18

22.68

2.00

3.80

7.03

9.52

2.50

2.90

4.23

5.49

3.00

2.43

2.94

3.65

3.50

2.14

2.23

2.63

4.00

1.95

1.80

2.00

4.50

1.80

1.51

1.59

5.00

1.69

1.31

1.30

5.50

1.60

1.16

1.09

6.00

1.53

1.05

0.93

6.50

1.46

0.97

0.81

7.00

1.41

0.90

0.71

7.50

1.37

0.85

0.63

8.00

1.33

0.80

0.57

8.50

1.29

0.77

0.52

9.00

1.26

0.74

0.47

9.50

1.23

0.71

0.44

10.00

1.21

0.69

0.41

10.50

1.18

0.67

0.38

11.00

1.16

0.65

0.36

11.50

1.14

0.64

0.34

12.00

1.12

0.63

0.32

12.50

1.11

0.62

0.30

13.00

1.09

0.61

0.29

13.50

1.08

0.60

0.28

14.00

1.06

0.59

0.27

14.50

1.05

0.58

0.26

15.00

1.04

0.58

0.25

15.50

1.03

0.57

0.24

16.00

1.02

0.57

0.23

16.50

1.01

0.56

0.23

17.00

1.00

0.56

0.22

17.50

0.99

0.56

0.21

18.00

0.98

0.55

0.21

18.50

0.97

0.55

0.20

19.00

0.96

0.55

0.20

19.50

0.96

0.54

0.20

20.00

0.95

0.54

0.19

20.50

0.94

0.54

0.19

21.00

0.93

0.54

0.19

21.50

0.93

0.53

0.18

22.00

0.92

0.53

0.18

22.50

0.92

0.53

0.18

23.00

0.91

0.53

0.18

23.50

0.90

0.53

0.17

24.00

0.90

0.53

0.17

24.50

0.89

0.52

0.17

25.00

0.89

0.52

0.17

25.50

0.88

0.52

0.17

26.00

0.88

0.52

0.16

26.50

0.87

0.52

0.16

27.00

0.87

0.52

0.16

27.50

0.87

0.52

0.16

28.00

0.86

0.52

0.16

28.50

0.86

0.52

0.16

29.00

0.85

0.51

0.16

29.50

0.85

0.51

0.15

30.00

0.85

0.51

0.15

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.