PKR39809-02

Local and Remote Control Modes

An important feature of the PowerLogic ADVC Controller is that it is always in one of two control modes, that is local or remote, and the work tag can be applied by local or remote operators.

The control mode and the tag provides operational safety by specifying the circumstances under which the ACR or AS can be closed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.