PKR39809-02

Terminology

ACR refers to the complete installation consisting of three major components that is switchgear, controller, and interconnecting cable. If the switchgear is a LBS and the controller is running sectionaliser firmware, the system is referred to as an AS. Where LBS is used in this document it refers to the switchgear component only.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.