PKR39809-02

Configuring the Quick Keys

The Quick Keys on the setVUE O.I. can be configured either via the O.I. or via WSOS.

Firstly, configurable quick keys must be made available through feature selection. This can be done on the O.I. if options are available by navigating to the Options – Controller 1 page in the system status menu.

That will cause the Quick Key Selection page below to be displayed, also in the system status menu. The fields on this page have the same positional arrangement as the quick keys on the O.I.

Select the first field to be changed and cycle through the available options until the required function is displayed and press the Menu key.

A set of stick-on labels are provided with each controller to change the text on the quick keys to match the new function.

The functions available for Quick Key selection are:

  • Cold Load

  • Live Load Blocking

  • LOCAL/Remote

  • Negative Phase Sequence (NPS) Protection

  • Reset Flags

  • Work Tag

  • Battery Test

  • Reverse Cold Load

  • Auto On/Off

  • Earth Protection

  • Protection Group

  • Blank (no function)

For details on how to configure the quick keys using WSOS, see Quick Keys.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.