PKR39809-02

Global OCP Settings

Right clicking the mouse with the cursor anywhere over the OCP display will open the Customize Global OCP Settings page.

Figure 49
Customize Global OCP Settings page

This dialogue can be used to:

  • Select and play the Beep Pattern.

  • Set the Flash On/Flash Off time settings for the lamps.

  • Select Universal Lamp Color Settings (leave unchecked if lamps are to be assigned colors individually).

  • Select a font for the display.

  • Select if the O.I. must turn On when the door is opened.

  • Select if a beep is required when a key or button is pressed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.