PKR39809-02

Protection Off

This setting turns off all of the protection features and therefore the ACR can only be tripped or closed manually.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.