PKR39809-02

SVIIS + TTS in Stand Alone Mode

The other option is to connect the SVIIS in series with the control cable between the switchgear port on the PowerLogic ADVC Controller and a TTS that is in stand alone mode. In this case the toggle switches would need to be in the Inject from Inputs position for voltage injection.

Points to note when testing with this configuration:

  • The switchgear is disconnected and the TTS is acting as a switchgear simulator.

  • The TTS contacts can be used for timing.

Figure 341
SVIIS and TTS connected in Stand Alone Mode

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.