PKR39809-02

Earth Fault (EF)

The EF elements are driven by the residual current that is the real-time vector sum of the three phase currents. The residual or earth current is calculated by digitally summing the phase currents sampled every 5 ms.

NOTE: The Zero Sequence Current (Io) is defined as Io = (Ia+ Ib+ Ic) / 3 Therefore the Zero Sequence Current (Io) is one third of the residual or earth current.

An EF pickup occurs when the measured current ≥ the earth setting current x the earth pickup multiplier. A tripping time is calculated based on the magnitude of the fault current and the settings for the active trip and updated every sample.

Unless the fault resets, a protection trip will ensue.

EF pickup, reset thresholds and multiplier settings are global that is they apply to all trips. Timing is determined by settings configured individually for Trips 1 – 4, Single Shot and Work Tag.

Configuration options for EF protection are listed in the table below.

Table 35 EF Protection Configuration Options

Phase overcurrent Configuration Settings

Range/Options

Resolution

Default

Global Settings

Setting Current

10...1260 A

1.0 A

40 A

Pickup Multiplier

1.0...10.0

0.1

1.0

Reset Threshold Multiplier

90...100%

10...100%(1)

1.0%

90%

Per Trip Timing Settings

Curve Options

Inverse Time Curves

3 x IEC255 Refer Appendix D

3 x IEEE Refer Appendix E

42 x TCC Refer Appendix F

Up to 5 User Defined Curves

IEC255 Standard Inverse

Other Curves

Definite Time Instantaneous Only

Inverse Time Curve Modifiers

Time Multiplier

0.01...25.00

.01

1.00

Instantaneous Multiplier

Off, 1.0...30.0

0.1

Off

Minimum Time

0.00...2.00 s

0.01 s

0.00 s

Additional Time

0.00...30.00 s

0.01 s

0.00 s

Maximum Time(1)

Off, 0.2...180.0 s

0.1 s

Off

Other Curves

Definite Time

0.01...100.00 s

0.01 s

1.00 s

Definite Time Instantaneous Multiplier

Off, 1.0...30.0 s

0.1 s

Off

Instantaneous Only

x 1.0...x 30.0

0.1

1.0

Instantaneous Minimum Time

0.00...2.00 s

0.01 s

0.00 s

(1) This is a global setting unless Extended Minimum Time per Curve is On.
(2) Reset Threshold Multiplier setting range is 10%...100% when Reset Curves are available.
 

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.