PKR39809-02

Options

When Options Available is selected on the System Settings 2 page as it is by default, another ten optional pages are added to the System Status display group.

The first four are related to Protection.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?