PKR39809-02

Protection Off Configuration

By default, Protection Off is not allowed. If it is required to turn protection off, Protection Off must be configured for allowed in either:

WSOS: Display > Configuration > Feature Selection> Protection or on the operator interface.

Once Protection Off has been made available, protection can be turned off in WSOS on the Control page.

When Protection is turned off, WSOS will display the message below:

An operator must select Yes in the above message to turn Protection Off.

Protection can also be turned Off via the O.I:

flexVUE: Operator Menu > Operator Controls > Auto Reclose On/Off Options for this setting field are:

  • Auto Reclose On

  • Auto Reclose Off

  • Protection Off

If protection is Off, selecting either Auto Reclose On or Auto Reclose Off will turn protection On.

setVUE: via the Auto Reclose On/Off field on Operator Settings 1 in the System Status menu.

Options for this setting field are:

  • Auto Reclose On

  • Auto Reclose Off

  • Protection Off

If protection is Off, selecting either Auto Reclose On or Auto Reclose Off will turn protection On.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.