PKR39809-02

Current

Phase angles shown on the Current page are relative to their respective phase voltages.

Current

     

A Phase current

20 A

-30°

Earth current

0 A

D

B Phase current

20 A

-30°

Positive Phase Sequence current

0 A

D

C Phase current

20 A

-30°

Negative Phase Sequence current

0 A

D

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.