PKR39809-02

SEF Wattmetric Polarizing

The Wattmetric method for SEF detection may be applied in all types of distribution systems having low EF values. This includes isolated-neutral high-impedance earthed and compensated systems.

The Wattmetric value is in Watts and is defined as the in-phase residual power given by:

Where Ø is the Fault Angle that is the angle between VZPS and IZPS. VZPS is the polarising voltage.

When Wattmetric is selected as the SEF Directional Blocking Decision WSOS displays this message:

This is because the SEF Pickup Threshold (Setting Current) is now in kilo Watts (kW) as shown below.

The Wattmetric SEF pickup threshold can be set between
0.01 kw and 10.0 kW.

SEF Wattmetric Characteristic Fault Angle

When a forward SEF occurs on a compensated earthing system, VZPS and IZPS are assumed to be 180° out of phase.

Therefore the Characteristic Angle for Wattmetric is fixed at 180°.

The Wattmetric Fault Angle for a given fault is the Zero Sequence Current angle relative to the Zero Sequence Voltage angle VZPS → IZPS.

The Angle at Fault recorded in the Event Log following a fault is the fault angle relative to the Characteristic Angle which is fixed at 180°.

So a fault with a Fault Angle (VZPS → IZPS) = 135° would log an Angle at Trip of -45° (135°-180°). Which indicates that the Fault Angle is lagging the Characteristic Angle by 45°.

When the Earth Tripping Direction is Trip Forward, the above fault will log the following events:

  • Forward Pickup SEF

  • SEF Directional Armed

  • SEF Protection Trip

  • Angle at Fault -45°

  • Quantity at trip Earth/SEF Wattmetric – xx.xx kW

  • Polarising Voltage at trip VZPS

  • Quantity at the maximum Earth/SEF – Maximum Wattmetric - xx.xx kW

  • Polarising Voltage at the maximum VZPS

SEF VZPS Sector Width

The default Forward and Reverse Sector Width settings for SEF protection are both 90°. These are ± settings and equate to actual sector widths of 180°.

Sector Width settings are identical for all elements and Decision settings. For more information, refer to Sector Width.

SEF Wattmetric Low Voltage Block

When the SEF Low Block setting is On, tripping is blocked if the polarising voltage is below the Low Threshold setting.

In this situation the ACR will still record fault resetting events when the apparent fault goes away as shown:

Fault On

  • SEF Directional Low VBlocked

  • Polarizing Voltage Low VZPS

Fault Off

  • Quantity at the maximum Earth/SEF – Maximum Wattmetric xx.xx kW

  • Polarizing Voltage at the maximum VZPS

When the Low Block setting is Off, the polarising voltage is disregarded and the action is entirely based on the calculated fault angle relative to the SEF Characteristic Fault Angle. So if the polarising voltage is below the SEF Low Threshold setting, a protection trip will occur but no fault angle will be logged.

The Event Log will record:

  • SEF Directional Low VArmed

  • Polarizing Voltage Low VZPS

  • SEF Protection Trip

  • SEF Low VZPS

  • Quantity at trip Earth/SEF Wattmetric xx.xx kW

  • Polarizing Voltage at trip VZPS

  • Quantity at the maximum Earth/SEF Wattmetric xx.xx kW

  • Polarizing Voltage at the maximum VZPS

The default SEF Low Threshold setting is 500 VZPS configurable over the range 150...15 000 VZPS.

SEF Wattmetric Voltage Memory

When Wattmetric is selected as the Decision for directional SEFs, a Voltage Memory time between 0.01 s and 10.00 s or OFF can be configured. The default setting is 2.00 s.

Consider a reverse SEF where VZPS and IZPS are in phase and VZPS is above the SEF Low Threshold setting.

If the SEF Tripping Direction is Trip Reverse, and the SEF Voltage Memory setting is 2.00 s, this fault will cause a reverse pickup and SEF Directional Armed will be logged.

If VZPS then drops below the SEF Low Threshold setting before the switchgear trips, this will not cause a Low V condition as the controller will continue to use the last sampled value of VZPS that was above the threshold as the polarising voltage while the pickup is active.

If the fault persists long enough to cause a trip, the memorized voltage and corresponding fault angle will be identified by an asterisk ‘*’.

The Event Log will report the following events:

  • Reverse Pickup SEF

  • SEF Directional Armed

  • SEF Protection Trip

  • Angle at Fault* 180°

  • Quantity at trip Earth/SEF Wattmetric xx.xx kW

  • Polarizing Voltage at trip* VZPS 514 V

  • Quantity at the maximum Earth/SEF Maximum Wattmetric xx.xx kW

  • Polarizing Voltage at the maximum VZPS 601 V

NOTE:
  • The Angle at Fault and Polarizing Voltage at trip events above are identified as memorized values.

  • The Polarizing Voltage at trip VZPS would be expected to be just above the Low Threshold setting (default 500 V).

  • The Polarizing Voltage at the maximum is not a memorized value as VZPS was above the Low Threshold setting when the fault first appeared.

SEF Wattmetric Fault Hold Time

When Wattmetric is selected as the Decision for directional SEFs, a Fault Hold Time between 0.01 s and 10.00 s or OFF can be configured. The default setting is 2.00 s.

The effect of the Fault Hold Time is to pause the protection timing for a set period after a fault that caused a pickup has gone away.

When the fault hold time is 2.00 s, a forward SEF with a tripping time of 3.0 s that goes away after 1.5 s for 1.0 s and then returns will cause a trip after another 1.5 s. Because the hold time, that is the time that the fault went away for (1.0 s), is a shorter duration than the Fault Hold Time (2.0 s), the pickup will remain active while protection timing is paused and the tripping time will be extended by the Fault Hold Time setting.

The Event Log will record a Paused event during the hold time.

The events recorded from pickup with relevant time stamps would be:

Event

Time Stamp

Forward Pickup SEF

00:00:00.00

SEF Directional Armed

00:00:00.00

All protection elements resetting

00:00:01.50

All protection elements paused

00:00:01.50

Protection element timing

00:00:02.50

SEF Protection Trip

00:00:04.00

Quantity at trip Earth/SEF Wattmetric xx.xx kW

00:00:04.00

Polarizing Voltage at trip VZPS

00:00:04.00

The fault was paused during the 1.0 s hold time so never reset. When the fault returned a Protection Element Timing event was logged.

NOTE: This was not a pickup as a pickup was already active.

The time between pickup and trip would be 4.0 s that is 3.0 s tripping time plus
1.0 s hold time.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.