PKR39809-02

LAN-1 and LAN-2

Table 18 Configuration settings for the LAN-1 and LAN-2 ports on the PowerLogic ADVC Controller

Setting

Description

Status

Indicates whether the port is in use by an application within the controller.

WSOS is permanently running on both of these ports by default.

Options: In Use, Enabled

Factory default is in use

This is a read-only field

Mode

Can be either Local or RM.

A port used for a SCADA protocol must be set to Remote.

IOEX could be either Local or Remote according to the application.

Used By

Displays the application that has been assigned to this port for example, WSOS, DNP3

Multiple applications can run on this port simultaneously.

WSOS is running on LAN-1 and LAN-2 ports by default.

Factory default is WSOS

This is a read-only field

Current Settings

These are the settings for this port currently in use by the controller.

All these fields are read-only

IP Address

Internet Protocol Address

The IP address of the controller.

Subnet Mask

The IP Subnet Mask of the controller

Default Gateway

The IP address of the controller’s default gateway.

DHCP

Dynamic Host Configuration Protocol

The DHCP mode of the controller.

If Enabled, the controller obtains its IP address and subnet mask from a DHCP server located on the network. The IP and subnet mask are not configurable.

If Disabled, the controller uses the IP address and subnet mask configured in the users settings.

New Settings

These fields show the settings to be applied. They are the same settings as those in the current settings above.

The IP and Subnet Mask settings are greyed out and cannot be changed if DHCP is checked.

If DHCP is not checked, the IP address and subnet mask must be configured by the user prior to selecting the Apply button.

If DHCP Enable is checked, selecting the Apply button will obtain an IP Address, Subnet Mask and Default Gateway from the DHCP server which will be applied.

Statistics

Receive Ethernet CRC Error Count

Displays the number of CRC error messages received since this count was last reset.

This field is read-only

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.