PKR39809-02

WSOS Measurements

System analogue measurements are displayed by WSOS on the Measurement page.

Display > Measurement

Figure 106
WSOS Measurements page

Per phase real, reactive, apparent power, and PF are displayed on a separate page along with Power Meter measurements.

This page can be opened by selecting the Display Power Measurement button on the measurement page.

Figure 107
Per Phase Power and Power Meter

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.