PKR39809-02

Close Retry

The Close Retry option enables Sync Check to issue a subsequent close request automatically when synchronism occurs sometime after an operator close was denied due to an out of sync condition. It helps to prevent the need for an operator to closely monitor the synchronization status of the system and issue another close request manually.

The Close Retry Period setting determines how long Close Retry will wait for the two sides to be synchronized after the initial close request.

While an automatic close request is pending, an alert message is displayed on the O.I.s showing the time remaining before the automatic close operation is aborted.

An operator may cancel a pending automatic close request by issuing a trip request or by changing any Sync Check setting.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.