PKR39809-02

Daily Maximum Demand

The controller maintains a log of Daily Maximum Demand records that show the total energy and peak power for each day. The most recent record i.e. the previous day, is displayed by default. The Date/Time displayed is the end of the period when the peak average power was logged.

Daily Maximum Demand

Previous Day

 

Total Energy for previous day (kWh)

 

Yesterday’s date

 

Date/Time for peak power

 
   

Peak power and power factor

 

Earlier records can be viewed by pressing the SELECT key to enter the history mode and navigating using the Left and Right Arrow keys.

When earlier records are being displayed, the title changes to:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.