PKR39809-02

Custom Menu with Rotation Mode Disabled

  • Pressing the MENU key at any time, will move the user out of the custom menu to the next standard menu display group.

  • Pressing the CUSTOM MENU key, will move the user to the next screen in the custom menu.

  • When displaying the custom menu screens, operation of the Quick Keys, the ALT key, the SELECT key and Arrow keys are as per standard display group behavior for example, SELECT key highlights a setting and Arrow keys move to the previous or next screen.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.