PKR39809-02

Sensitive Earth Fault (SEF)

SEFs are low level earth faults < 80 A primary.

The SEF elements are driven by measured residual current. The residual current used for the SEF element is determined by measuring the current in the common connection between the three CT secondary currents on the PCOM board.

Residual current = A phase current + B phase current + C phase current or
Ie= Ia+ Ib+ Ic

NOTE: Zero Sequence Current (Io) is defined as Io = (Ia+ Ib+ Ic) / 3 Therefore the Zero Sequence Current (Io) is one third of the residual or earth current.

A SEF pickup occurs when the measured current ≥ the SEF setting current x the SEF pickup multiplier. A tripping time is calculated based on the magnitude of the fault current and the settings for the active trip and updated every sample.

Unless the fault resets, a protection trip will ensue.

SEF pickup, reset thresholds and multiplier settings are global that is they apply to all trips. Timing is determined by settings configured individually for Trips 1...4, Single Shot and Work Tag.

Configuration options for SEF protection are listed in the table below.

Table 36 SEF Protection Configuration Options

Phase O/C Configuration Settings

Range/Options

Resolution

Default

Global Settings

Setting Current

10...1260 A

1.0 A

4 A

Pickup Multiplier

1.0...10.0

0.1

1.0

Reset Threshold Multiplier

90...100%

10...100%(2)

1.0%

90%

Per Trip Timing Settings

Curve Options

Inverse Time Curves

3 x IEC255 Refer Appendix D

3 x IEEE Refer Appendix E

42 x TCC Refer Appendix F

Up to 5 User Defined Curves

Definite Time

Other Curves

Definite Time Instantaneous Only

Inverse Time Curve Modifiers

Time Multiplier

0.01...25.00

.01

1.00

Instantaneous Multiplier

Off, 1.0...30.0

0.1

Off

Minimum Time

0.00...2.00 s

0.01 s

0.00 s

Additional Time

0.00...30.00 s

0.01 s

0.00 s

Maximum Time(1)

Off, 0.2...180.0 s

0.1 s

Off

Other Curves

Definite Time

0.01...100.00 s

0.01 s

1.00 s

Definite Time Instantaneous Multiplier

Off, 1.0...30.0 s

0.1 s

Off

Instantaneous Only

x 1.0...x 30.0

0.1

1.0

Instantaneous Minimum Time

0.00...2.00 s

0.01 s

0.00 s

(1) This is a global setting unless Extended Minimum Time per Curve is On.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.