PKR39809-02

Protection Trip

A protection trip occurs when the controller sends a trip signal to the circuit breaker in response to a fault it has detected on the feeder. A protection trip may or may not lead to an automatic reclose depending on the configuration settings stored in the controller.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.