PKR39809-02

SEF Directional Block

SEF Directional Blocking works the same way as EF and can use the same three methods to determine the direction of a SEF.

  • VZPS

  • Wattmetric

  • Ir Cos (Ø)

VZPS is the default option. The Decision setting determines the method used. Operating Quantities, Fault Angles, and default Characteristic Angles for each method are shown in the table below.

Table 80 Directional Blocking SEF Polarizing Methods

Polarizing Method (Decision)

Operating Quantity

Fault Angle

Angle logged on Trip

Default Characteristic Angle

VZPS

Earth Current (Ir)

VZPS → IZPS

VZPS → IZPS

135° Configurable

Wattmetric

Residual Power

VZPS x IZPS x Cos (FA)

VZPS → IZPS

(VZPS → IZPS) – CA (180°)

180° Fixed

Ir Cos (Ø)

Active Earth Current

IZPS x Cos (FA)

VZPS → IZPS

-VZPS → IZPS – CA (180°)

180° Fixed

Tripping direction options for SEFs regardless of the polarising method are:

  • Trip Forward

  • Trip Reverse

  • Trip Forward and Reverse (that is non directional)

SEF has a default setting current of 4 A and can be configured for between 1 A and 80 A.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.