PKR39809-02

Overview

The SCADA Output Control Mode enables Local/Remote control of all SCADA binary and analogue outputs (controls).

When the SCADA Output Control Mode is enabled, placing the PowerLogic ADVC Controller in local control mode helps to prevent remote SCADA operators from operating the switchgear or performing any other controls.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.