PKR39809-02

Sync Check Settings Displays

Once Sync Check has been made available for an ACR, a Sync Check settings page is added to the protection settings for each protection group in WSOS.

Figure 227
WSOS Sync Check settings for an ACR

Making Sync Check available for an AS adds a Sync Check setting page for each detection group.

Figure 228
Sync Check settings for an AS

Making Sync Check available also adds a Sync Check sub-menu on the flexVUE O.I. for an ACR and AS.

Four Sync Check setting pages are added to the setVUE O.I. for both ACR and AS.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.