PKR39809-02

Single Shot Summary

  • An ACR will go directly to Lockout following a protection trip if it is in Single Shot mode.

  • Providing the Work Tag has not been applied, an ACR will be in Single Shot mode if:

    • Auto Reclose is Off.

    • An operator has closed the device. Providing the Single Shot Reset Timer has not been set to zero.

  • The timing of a trip that occurs when the ACR is in Single Shot mode is determined by dedicated Single Shot settings for the particular type of fault.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.