PKR39809-02

Connect the FTIM to the controller

  1. Before connecting the FTIM, turn off all power to the controller.

  2. Connect the shielded 15 pin D connector to the FTIM.

  3. Fasten the connector securely helps to ensure a reliable connection.

  4. Turn all power to the controller ON when the installation is complete.

    Figure 328
    FTIM with 15 pin D connector fitted

NOTE: Failure to power OFF the controller when connecting the FTIM to the CAPE may cause unwanted trip/close operation.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.