PKR39809-02

Setting Change Events

The PowerLogic ADVC Controller logs all setting changes regardless of the source. Pressing the ALT key when setting changes are being displayed in the event log will display not only the source but also extra information that could include the protection group, curve and trip number. Pressing the ALT again will return the Event Log display to normal including Date/Time stamps.

In the above example, extra information regarding setting changes was displayed.

Event 1 (top) – The O.I. was used to change the displayed protection group from A to B.

Event 2 – The O.I. was used to change the Phase Trip setting from Group B to 205 Amps.

Event 3 – WSOS was used to change the Earth Trip setting for Group C to 50 Amps.

Event 4 (bottom) – WSOS was used to change the Phase Trip 1 protection curve in Group A to IEC255 standard Inverse.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.