PKR39809-02

ACO Communications

Failure during changeover process On

Selecting this option changes ACO Status to Aborted/Not Ready/Waiting if the primary device does not send the trip or close request during a changeover or restoration sequence. In this scenario, ACO Status reads:

WSOS5

O.I.s

Status: DEVICE has failed to Trip or Close

Status: DEVICE failed to Trip or Close

Ping failure On

Selecting this option changes ACO Status to Aborted/Not Ready/Waiting if the primary device does not receive a ping response from the secondary device or the secondary device does not receive a keep-alive signal from the primary device. In this scenario, ACO Status reads:

WSOS5

O.I.s

Status: DEVICE is not responding to communications

Status: DEVICE comms not responding

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.