PKR39809-02

Single Sided CVT Switchgear

UOV protection may be used on a PMSet U Series ACR with voltage measurement on only one side but Normal Voltage Close can only be configured if the voltage measurement is on the designated Source side.

If Normal Voltage Close is On when the Source/Load designation is changed it will be forced Off.

If the Source/Load designation is changed while a normal voltage close is pending, the ACR will go to Lockout.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.