PKR39809-02

Appendix K.1 ­ setVUE ACR Menu Structure

The setVUE displays are organized into logical groups called Display Groups. Within each group is a menu of pages and some pages have sub-pages.

Figure 356
setVUE Menu Structure

The Automatic display group only appears if an automation feature i.e. Loop Automation or Auto Changeover is available. Otherwise the display will move from Protection directly to the Communications display group.

Pressing the MENU key causes the display to move to the next group in turn.

The Left and Right Arrow keys are used to scroll through the screens within a display group.

All display groups are circular. So pressing the Right Arrow key when the last screen in the group is being displayed will cause the display to return to the first screen.

The individual screens in each of the display groups are shown in Appendices K.2 to K.6

The following table represents the procedure to find the settings on the
setVUE O.I.

Table 140 Finding an ACR setting on the setVUE O.I.

Step

Action

1.

Press MENU until the menu group you require is displayed on the screen.

Example: PROTECTION.

2.

Use the arrow keys to scroll through until you find the required menu.

Example: PROTECTION SETTINGS > Directional Blocking 3

3.

On that menu is the setting you are looking for.

Example: Minimum Vzps

4.

For information on changing settings refer to Chapter 4 Operator Functions.

The structure of the setVUE menu changes when the Custom Menu is used.

Figure 357
setVUE Custom Menu

When the Custom Menu has been configured using WSOS it can be accessed by pressing the Custom Menu key on the operator interface.

Continuing to press the Custom Menu key will cause the display to step through the selected screens.

Alternatively the display may have been configured to scroll automatically when the operator interface is on.

Pressing the Custom Menu key will have no effect if it has not been configured.

The display will return to the main menu if the Menu key is pressed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.