PKR39809-02

Document Scope

This manual describes the operation of the PowerLogic ADVC Controller Range. While every care has been taken in the preparation of this manual, no responsibility is accepted for loss or damage incurred by the purchaser or user due to an error or omission in this document. Inevitably, not all details of equipment are provided, nor are instructions for every variation or contingency during installation, operation, or maintenance. For additional information on specific problems or requirements, contact the manufacturer or your distributor.

Automatic Circuit Reclosers using the PowerLogic ADVC Controller

An Automatic Circuit Recloser (ACR) is a system consisting of a controller (PowerLogic ADVC Controller) and appropriate switchgear connected by an umbilical control cable. The switchgear needs to be capable of breaking fault current that is a circuit breaker.

Automatic Sectionalisers using the PowerLogic ADVC Controller

An Automatic Sectionaliser (AS) is a system consisting of a controller and appropriate switchgear connected by an umbilical control cable. The switchgear may be either a Load Break Switch (LBS) or a circuit breaker.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.