PKR39809-02

USB-1, USB-2, and USB-3

The PowerLogic ADVC Controller comes with 3 general purpose USB 2.0 Type A ports, which are USB-1, USB-2, and USB-3.

Figure 62
USB Type A Port

These ports can be configured to use a suitable USB-RS232 converter, must there be need for additional RS232 ports. Any of the protocols, which can be configured to run on the RS232 port, can then be configured to run off the
USB-1/2/3 ports, with a converter attached.

The pinout for all these ports are according to the USB2.0 specification as shown in the below table:

Table 15 USB Type A port pin out

Pin

Name

Description

1

VBUS

+5V

2

D-

Data -

3

D+

Data +

4

GND

Ground

The USB Type A ports are not isolated from one another or from the controller electronics. They therefore can only be connected to devices inside the controller that are powered by the controller radio supply, including modems, optical isolators, and radios.

NOTICE
HAZARD OF USB ERROR
When using a USB adaptor, it is strongly recommended that the adaptor be tested on a PC first, to make sure that it is functional and not damaged/faulty.
Failure to follow these instructions can result in equipment damage.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.