PKR39809-02

Per Phase Power Measurements

The dialogue box that opens in WSOS when Display Power Measurement is clicked on the Measurement page also displays per phase power measurements.

Real time measurements for Real (kW), Reactive (kVAR), Apparent (kVA) Power and PF are displayed on a per phase basis.

Apart from Apparent Power, these measurements are also displayed on the operator interface.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.