PKR39809-02

Time Zone and Daylight Saving Events

Any changes to the time zone or daylight saving settings will be recorded in the event log when they are enabled. Events are also logged to record the start and end of the daylight saving period.

Some examples of these events are shown in the figure below:

Figure 45
Sample of Time Zone and Daylight Saving Events

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.