PKR39809-02

Event Log on setVUE

On the setVUE O.I., the event log display group is one of the main display groups shown in Appendix K.1 setVUE Menu Structure.

To view the Event Log on the setVUE O.I., press MENU until the title line displays EVENT LOG with the letter E in the top right hand corner.

When the Event Log is initially displayed, the three most recent events are shown with the most recent on the bottom line. The title line will disappear and four events will be displayed once the Left Arrow key is pressed. From there, the event log can be scrolled for earlier and more recent events using the Left and Right Arrow keys. If the event log is scrolled back to the most recent event, the title line will reappear.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.