PKR39809-02

Other Context Menu Options

Other context menu options include Copy, Find and Go to Date/Time which can assist in finding particular events.

Display Source adds an extra column to the display that includes the source of individual events.

Selecting the Event Log Filter will open the Event Log Filter dialogue box shown below.

Figure 263
Event Log Filter

Using this dialogue, filters can be applied according to the Sources of the events, the time period the events occurred or any words to include or exclude. AND and/or OR logic can be applied to entered words.

When two events have been selected by holding down the Ctrl key on the keyboard, the Display Time Difference option can be used to measure the elapsed time between events. This can be useful for measuring protection trip timing.

Figure 264
Display Time Difference

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.