PKR39809-02

Display Groups

The O.I. displays are organized into three logical groups. Within each group is a menu of pages and those menus have various sub-menus. An overview of the default flexVUE menu structure is shown in the Figure 15.

Figure 15
flexVUE O.I. Menu structure

Pressing the MENU key will always bring the display back to the main menu page from where any of the three main menu display groups can be selected and entered.

The three main menu display groups that can be displayed on the flexVUE O.I. LCD display are described below.

ALERTS MENU

  • This group displays Normal Alerts which are meant to warn operators that an abnormal condition exists. A normal alert could be to warn the operator that the close circuit switch is in the disable position. This would sound an alarm and cause an Alerts Active message to alternate with the title line on the display.

  • Pressing the right arrow key when the alert is active will enter the Alerts Menu and display details of the active alert.

NOTE: The PowerLogic ADVC Controller can also generate Critical Alerts to warn of an imminent trip/close operation or trip/close coil failure. These alerts have nothing to do with the Alerts menu. No menu navigation is possible when a critical alert is active but the QAKs can be used

OPERATOR MENU

  • Pressing the right arrow key when the above page is displayed will enter the Operator Menu and allow access to the operator sub-menus.

  • The Operator Menu contains all of the displays and settings required for routine operation of the device.

ENGINEER MENU

  • Pressing the right arrow key when the above page is displayed will enter the Engineer Menu and allow access to the Engineer sub-menus.

  • The Engineer Menu contains more comprehensive metering as well as historical displays and allows access to all the settings required to configure all of the protection, communications and control functions.

For a complete listing of pages in the flexVUE menus refer to Appendix J flexVUE Menu.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.