PKR39809-02

IOEX Inputs

The IOEX 6 Input shown in the figure below must be hardwired permanently High but is only asserted when its logic is True.

The logic requires Inputs 2, 3, and 4 to be wired to go High when they receive trip confirmation signals from DG devices 1, 2, and 3 respectively.

Alternatively, trip confirmation signals can be bypassed by Protocol IOEX controls.

Figure 154
IOEX Input for Conditional Auto Reclose map

The logic for the IOEX Inputs is shown in the figure below.

NOTE: Each input is OR’d with a protocol IOEX control that can be used to bypass individual DG devices if required.

Figure 155
Conditional Auto Reclose IOEX Input Logic

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.