PKR39809-02

Automatic Protection Group Selection (APGS)

APGS can be used to automatically change the active protection group to suit the network configuration without the need for operator intervention.

APGS works by automatically changing between protection groups depending on the direction of power flow through the switchgear.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.