PKR39809-02

EF Directional Blocking

The tripping direction for EFs may be:

  • Trip Forward

  • Trip Reverse

  • Trip Forward and Reverse (that is non directional)

When EF Directional Blocking is used, one of three methods can be used to determine the direction of an EF.

  • VZPS

  • Wattmetric

  • Ir Cos (Ø)

VZPS is the default option. The Decision setting determines the method used. Operating Quantities, Fault Angles and default Characteristic Angles for each method are shown in the table below.

Table 47 Directional Blocking EF Polarizing Methods

Polarizing Method (Decision)

Operating Quantity

Fault Angle

Angle logged on Trip

Default Characteristic Angle

VZPS

Earth Current Ir (IZPSx3)

VZPS → IZPS

VZPS → IZPS

135° Configurable

Wattmetric

Residual Power

(VZPSx3) x (IZPSx3) x Cos (FA)

VZPS → IZPS

(VZPS → IZPS) – CA (180°)

180° Fixed

Ir Cos (Ø)

Active Earth Current

(IZPSx3) x Cos (FA)

VZPS → IZPS

-VZPS → IZPS – CA (180°)

180° Fixed

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.