PKR39809-02

Unlock Key

Unless configured otherwise, QAKs are normally locked helps to prevent accidental QAKation. To use the QAKs, an QAKator must first press the Unlock key. The lamp above the unlock key will be green (default) while the QAKs are active. To deactivate the QAKs an operator can press the unlock key again. The lamp will turn red (default).

Alternatively, the QAKs will be deactivated automatically a short configurable delay (default 10 s) after the last QAK was selected.

To customize the Quick Action Unlock key, place the cursor over the padlock symbol and click the left mouse button. This will open the Customize Unlock Key dialogue box.

Figure 54
Customize Unlock Key page

This dialogue can be used to change the time out period as well as the colors that indicate QAKs are locked and unlocked.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.