PKR39809-02

IEC 60870-5-104

There is a five-step procedure required to enable the PowerLogic ADVC Controllerto communicate with a SCADA master station using the IEC 60870-5-104 protocol:

  1. Check that IEC 60870-5-101/4 and TCP/IP are available.

  2. Select a communications port for IEC 60870-5-104.

  3. Configure the communications settings for the selected port.

  4. Assign the selected port to IEC 60870-5-104.

  5. Configure the IEC 60870-5-104 settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.