PKR39809-02

Standards and Guidelines

The Sync Check functionality it the PowerLogic ADVC Controller Range complies with the requirements of IEEE 1547-2003 standard section 5.1.2 A – Synchronous interconnection to a EPS, or an energized local EPS to an energized Area EPS.

Table 88 IEEE 1547 – 2003 EPS/DR Interconnection Requirements

Aggregate rating of DR units (kVA)

Frequency difference (∆f,Hz)

Voltage difference (∆V, %)

Phase angle difference (∆Ø, °)

0–500

0.3

10

20

500–1500

0.2

5

15

1500-10000

0.1

3

10

It also complies with the requirements of major diesel generation device vendors:

Table 89 Diesel generator vendor guidelines for synchronous interconnection

Frequency difference (∆f,Hz)

ROCOF (Hz/s)

Voltage difference (∆V, %)

Phase angle difference (∆Ø, °)

0.1 Hz

0.1 Hz/s

3% Generator-Mains

5° Daily Interconnections*

0.5% Generator - Generator

10° Infrequent Interconnections

15° Gas Engine Interconnection

More information on the Sync Check feature for the PowerLogic ADVC Controller can be found in the Sync Check Technical Manual.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.