PKR39809-02

Introduction

This feature works in conjunction with either the DNP3 or IEC 60870-5-101/4 communications protocols.

When Protocol Monitor is enabled, the PowerLogic ADVC Controller will cycle the power to the communications peripheral device if it detects that the protocol has stopped communicating with the master station. This forces a re-initialisation of the communications device. The duration for which the peripheral communication device is without power is configurable.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.