PKR39809-02

NPS Characteristic Fault Angle

The Characteristic Fault Angle is the expected fault angle for a forward NPS overcurrent fault.

For NPS protection, the Characteristic Angle can be configured for a value between -179° and 180°.

120° is the default Characteristic Angle for NPS faults. So an NPS fault where the NPS current INPS leads the NPS voltage VNPS by 120° would be a forward fault in the centre of the forward sector.

When the Tripping Direction is forward and the Forward Sector Width is the default 90°, NPS faults with fault angles between 30° and 210° (-150°) would cause NPS Directional Protection to Arm and potentially trip.

The Angle at Fault reported in the Event Log would be 120°.

The Event Log will also record:

  • Pickup NPS

  • NPS Directional Armed

  • NPS Protection Trip

  • Angle at Fault 120°

  • Polarising Voltage at Trip VNPS

  • Polarising Voltage at the Maximum VNPS

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.