PKR39809-02

Changing Protection Settings on setVUE

Protection settings on the setVUE O.I. are password protected. To change a protection setting, follow the steps detailed in the Operator Settings section above. In addition, enter the password when prompted. When the setting change is completed by pressing ENTER, the following message will flash at the top of the screen:

At this point, the changed setting will be displayed but not in service. If further setting changes are required, they can be made now.

When all of the required setting changes are completed, press ENTER.

The following text will be displayed:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.