PKR39809-02

Earthing the SVIIS

An earthing stud terminal, complete with wing nut, is provided at the side of the SVIIS.

Make sure that the SVIIS is correctly earthed before commencing test procedures involving hazardous voltages.

All earthing must be in accordance with the supply authorities authorized practices and procedures.

Figure 342
SVIIS Earth Stud

NOTE: The Secondary Voltage Injection Interface Set is purchased as a separate item. For further information, refer to Schneider Electric or your local distributor.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.