PKR39809-02

Phase Compensation

The Phase Compensation option allows the time to close the switchgear to be taken into account when the system issues the close request. Depending on the frequency difference and phase difference between the two sides, Sync Check will determine when the close request needs to be issued in order for the actual closing of the switchgear contacts to occur when the two supplies are perfectly synchronized.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.