PKR39809-02

USB WSOS

The USB WSOS port is dedicated to running the WSOS software and cannot be used for any other purpose.

Connect a PC running WSOS to this port using a USB Type A to Type B cable.

The connector is a USB type B socket with the following pinout.

Table 14 USB WSOS Port Pin Connections

Pin No.

Name

Description

1

Vcc

+ 5 VDC

2

D-

Data -

3

D+

Data +

4

Gnd

Ground

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.