PKR39809-02

V0 Pickup Threshold

If the measured zero sequence voltage exceeds the V0 Pickup Threshold setting value it will trigger a GFN pickup condition.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.