PKR39809-02

Inrush Restraint Summary

  • Inrush Restraint helps to prevent the ACR from tripping unnecessarily due to short lived inrush current such as magnetizing current associated with energizing a transformer.

  • Pickup and Max Current events are still logged according to the Fault Detect setting for each element even though the Inrush Multiplier is being applied.

  • Inrush Restraint affects Phase, Earth, and NPS protection but does not apply to Definite Time or SEF protection.

  • Inrush Restraint is triggered by currents going from zero to non-zero. So if normal load currents are expected to drop below 2.5 A Inrush cannot be used and must be left off.

Table 43 Inrush Restraint Settings/Specifications

Inrush Restraint Settings/Specifications

Inrush Restraint Multiplier Range

1...30

Inrush Restraint Multiplier Resolution

0.1

Inrush Restraint Time Range

0.05...30 s

Inrush Restraint Time Resolution

0.01

Timing Accuracy

± 20 ms

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.