PKR39809-02

ACO Settings Displays

Once ACO has been made available, an ACO configuration page is added to the Display menu.

Display > ACO > ACO Configuration

When this page is first opened it is displayed with a Rank of secondary by default as shown in the figure below.

Figure 253
WSOS ACO Configuration secondary settings

Additional settings are required to be configured when the Rank of the device is primary.

Figure 254
WSOS ACO Configuration primary settings

If ACO is available it can also be configured on the operator interface.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.